STRINGS.IPMODERESET
Description
If the AKD-N’s connected to the AKD-C are set to an invalid static ip address, the command STRINGS.IPMODERESET on the AKD-C can be used to reset the ip mode of all AKD-Ns. After execution of this command, the AKD-N retrieve a new IP address either through DHCP or Auto IP.
-
- This command will only effect AKD-N’s with FW version greater or equal to M_01-14-00-003.
General Information
Type |
Command |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
N/A |
Start Version |
M_01-14-00-003 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD Profinet | No |
AKD sercos® III | No |
AKD-N | No |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics
The AKD-C Central Power Supply