STRINGS.STOSTATEMASK
Description
STRINGS.STOSTATEMASK reads which strings have drives with remote STO connected. Each bit represents one string, starting with string 1 in the least significant bit.
Value | Description |
---|---|
0 | No drives with remote STO connected |
1 | At least one drive with remote STO connected |
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
0 to 255 |
Default Value |
N/A |
Data Type |
Integer |
Start Version |
M_01-016-04-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD Profinet | No |
AKD sercos® III | No |
AKD-N | No |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics
The AKD-C Central Power Supply