TEMP.POWER1 to TEMP.POWER3

Description

Reads the temperature of the power board(s) temperature sensor(s). Most AKDs have only one power board sensor which is read by TEMP.POWER1.

General Information

Type

R/O Parameter

Units

Degrees Celsius

Range

-127 to 128

Default Value

N/A

Data Type

Integer

Start Version

M_01-09-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
TEMP.POWER1

PROFINET

2875 Word Yes
Sercos® III 2 Octets
TEMP.POWER2

PROFINET

2876 Word
Sercos® III 2 Octets
TEMP.POWER3

PROFINET

2877 Word
Sercos® III 2 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
TEMP.POWER1 876 2 Byte Signed Integer
TEMP.POWER2 877
TEMP.POWER3 878
Modbus
Parameter Register Address Is 64 bit? Attributes Signed? Object Start Version
TEMP.POWER1 1750 No 16-bit Yes

M_01-06-03-000

TEMP.POWER2 1752
TEMP.POWER3 1753

Related Topics

DRV.TEMPERATURES | TEMP.CONTROL