UNIT.VLINEAR
Description
UNIT.VLINEAR sets the units type for the velocity parameters when the motor type (MOTOR.TYPE) is linear.
Type | Description |
---|---|
0 |
Counts per second |
1 |
Millimeters per second |
2 |
Micrometers per second |
3 |
(Custom Units) per second |
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
0 to 3 |
Default Value |
0 |
Data Type |
Integer |
See Also |
|
Start Version |
M_01-00-00-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD PROFINET | Yes |
AKD Sercos® III | Yes |
AKD-N | Yes |
AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Index/Subindex | Object Start Version |
---|---|
518Ah /0 |
M_01-00-00-000 |
Fieldbus | Address | Attributes | Signed? |
---|---|---|---|
PROFINET |
2394 | Byte | No |
Sercos® III | 2 Octets |
Instance | Data Size | Data Type |
---|---|---|
395 | 1 Byte | Integer |
Register Address | Is 64 bit? | Attributes | Signed? | Object Start Version |
---|---|---|---|---|
788 |
No | 8 bit | No |
M_01-03-00-000 |
Related Topics