USER.INT1 to USER.INT24

Description

This parameter stores an integer value. To retain this value after a power-cycle, a "Save to Device" command must be performed from the Parameter Load/Save view in WorkBench.

General Information

Type

R/W Parameter

Units

N/A

Range

-2,147,483,648 to 2,147,483,647

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
USER.INT1

PROFINET

2497 DWord Yes
Sercos® III 4 Octets
USER.INT2

PROFINET

2498 DWord
Sercos® III 4 Octets
USER.INT3

PROFINET

2499 DWord
Sercos® III 4 Octets
USER.INT4

PROFINET

2500 DWord
Sercos® III 4 Octets
USER.INT5

PROFINET

2501 DWord
Sercos® III 4 Octets
USER.INT6

PROFINET

2502 DWord
Sercos® III 4 Octets
USER.INT7

PROFINET

2503 DWord
Sercos® III 4 Octets
USER.INT8

PROFINET

2504 DWord
Sercos® III 4 Octets
USER.INT9

PROFINET

2505 DWord
Sercos® III 4 Octets
USER.INT10

PROFINET

2506 DWord
Sercos® III 4 Octets
USER.INT11

PROFINET

2507 DWord
Sercos® III 4 Octets
USER.INT12

PROFINET

2508 DWord
Sercos® III 4 Octets
USER.INT13

PROFINET

2509 DWord
Sercos® III 4 Octets
USER.INT14

PROFINET

2510 DWord
Sercos® III 4 Octets
USER.INT15

PROFINET

2511 DWord
Sercos® III 4 Octets
USER.INT16

PROFINET

2512 DWord
Sercos® III 4 Octets
USER.INT17

PROFINET

2513 DWord
Sercos® III 4 Octets
USER.INT18

PROFINET

2514 DWord
Sercos® III 4 Octets
USER.INT19

PROFINET

2515 DWord
Sercos® III 4 Octets
USER.INT20

PROFINET

2516 DWord
Sercos® III 4 Octets
USER.INT21

PROFINET

2517 DWord
Sercos® III 4 Octets
USER.INT22

PROFINET

2518 DWord
Sercos® III 4 Octets
USER.INT23

PROFINET

2519 DWord
Sercos® III 4 Octets
USER.INT24

PROFINET

2520 DWord
Sercos® III 4 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
USER.INT1 498 4 Byte Signed Integer
USER.INT2 499
USER.INT3 500
USER.INT4 501
USER.INT5 502
USER.INT6 503
USER.INT7 504
USER.INT8 505
USER.INT9 506
USER.INT10 507
USER.INT11 508
USER.INT12 509
USER.INT13 510
USER.INT14 511
USER.INT15 512
USER.INT16 513
USER.INT17 514
USER.INT18 515
USER.INT19 516
USER.INT20 517
USER.INT21 518
USER.INT22 519
USER.INT23 520
USER.INT24 521
Modbus
Parameter Register Address Is 64 Bit? Attributes Signed? Object Start Version
USER.INT1 994 No 32 Bit Yes M_01-00-00-000
USER.INT2 996
USER.INT3 998
USER.INT4 1000
USER.INT5 1002
USER.INT6 1004
USER.INT7 1006
USER.INT8 1008
USER.INT9 1010
USER.INT10 1012
USER.INT11 1014
USER.INT12 1016
USER.INT13 1018
USER.INT14 1020
USER.INT15 1022
USER.INT16 1024
USER.INT17 1026
USER.INT18 1028
USER.INT19 1030
USER.INT20 1032
USER.INT21 1034
USER.INT22 1036
USER.INT23 1038
USER.INT24 1040