VBUS.HALFVOLT

Description

This parameter changes operational voltage thresholds inside the drive to allow operation at lower voltage thresholds to operating with half of the normal input ac line voltage.

For information on voltage ratings and drive types see AKD Models.

When the VBUS.HALFVOLT value is changed, the revised thresholds take effect immediately.

Value Description
0 Standard voltage rating
1 Reduced voltage rating

When changing this parameter, it impacts the following voltage-thresholds:

Drive Type AKD-xzzz06

Voltage Thresholds VBUS.HALFVOLT Value
0 1
DC-bus overvoltage fault threshold (see VBUS.OVFTHRESH) 420 VDC 210 VDC
Minimum undervoltage level threshold (see VBUS.UVFTHRESH) * 90 VDC 90 VDC
Regeneration thresholds 380-400 VDC 190-200 VDC

Drive Type AKD-xzzz07

Voltage Thresholds VBUS.HALFVOLT Value
0 1
DC-bus overvoltage fault threshold (see VBUS.OVFTHRESH) 840 VDC 420 VDC
Minimum undervoltage level threshold (see VBUS.UVFTHRESH) * 380 VDC 90 VDC
Regeneration thresholds 760-800 VDC 380-400 VDC

  • The DC-bus under voltage fault threshold (see VBUS.UVFTHRESH) is a user selectable command. It means that the user is responsible for setting the under voltage threshold to a proper value in case that the AKD is supplied with a lower DC-bus voltage than the rated voltage.

The regeneration thresholds describe the voltages when the drive generates regen power. The table above provides the voltage range for drive type -06 and -07. The lower voltage level is the level at which the drive starts generating regen power, the higher voltage level is the level at which the regen power is at 100%.

The inrush-relay open / close voltage thresholds are adapted automatically in relation to the minimum undervoltage threshold.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

N/A

Start Version

M_01-04-01-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

5261h /0

M_01-04-01-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2609 Byte No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
610 1 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed?
1218 No 8 bit

No