VBUS.PHASESTATE
Description
VBUS.PHASESTATE displays which input phases are connected to the device. Each bit represents one phase, starting with phase 1 in the least significant bit. The bit is set when the phase is connected.
Example
Only phases 1 and 2 are connected. VBUS.PHASESTATE will read 3 (binary 011).
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
0 to 7 |
Default Value |
N/A |
Data Type |
Integer |
Start Version |
M_01-18-02-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD Profinet | No |
AKD sercos® III | No |
AKD-N | No |
AKD-C | Yes |
Fieldbus Information
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
3088 |
No | 8-bits | No |
M_01-18-02-000 |