VBUS.VALUE

Description

VBUS.VALUE reads the DC bus voltage.

General Information

Type

R/O Parameter

Units

VDC

Range

0 to 900VDC

Default Value

N/A

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen

Index/Subindex Object Start Version
361Ah/0 M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2403 DWord Yes
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
404 4 Byte Signed Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

806

No 32 bit No M_01-03-00-000

Related Topics

"Regeneration"