VL.BUSFF
Description
Displays the velocity loop feedforward value injected by the fieldbus. Only active in position mode.
General Information
Type |
R/O Parameter |
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR Rotary: rpm, rps, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, µm/s, (custom units)/s |
Range |
0.0 to VL.LIMITP |
Default Value |
0.0 |
Data Type |
Float |
See Also |
|
Start Version |
M_01-00-00-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
EtherCAT COE and CANopen |
60B1h /0 |
M_01-00-00-000 |
Fieldbus |
Parameter |
Address |
Attributes | Signed? |
---|---|---|---|---|
Profinet |
VL.BUSFF_32 |
2424 |
DWord | Yes |
sercos® III | 8 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 425 | 8 Byte Signed | Velocity |
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
848 |
Yes | low 32 bit word | Yes |
M_01-03-00-000 |
Related Topics