VL.FBDISPLAY
Description
VL.FBDISPLAY returns the low pass filtered velocity feedback signaled based on the raw incremental position values. The cutoff frequency for the filter can be configured by VL.FBDISPLAYCUTOFF.
The signal is independent of the drive tuning parameter and might be useful for display purposes in HMIs.
General Information
Type |
R/O Parameter |
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR Rotary: rpm, rps, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, µm/s, (custom units)/s |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
See Also |
|
Start Version |
M_01-19-02-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
EtherCAT COE and CANopen |
N/A |
N/A |
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
3155 |
DWord | Yes |
sercos® III | 8 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 1156 | 4 Byte Signed | Velocity |
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
3126 |
Yes | 64 Bit | Yes |
M_01-19-02-000 |