VL.THRESHCUTOFF
Description
The parameter VL.THREHCUTOFF can be used to filter the over speed signal that is used for fault F302 generation.
The default value 0 means that there is no filtering, and the over speed signal is similar to VL.FBUNFILTERED .
A value over zero means a low pass filtered version of the VL.FBUNFILTERED signal is used for the over-speed detection. This can be useful in applications with “low” resolution encoders like resolver.
General Information
Type |
NV Parameter |
Units |
Hz |
Range |
0 to 2000 |
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-16-01-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD Profinet | Yes |
AKD sercos® III | Yes |
AKD-N | Yes |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
EtherCAT COE and CANopen |
53FDh/0 |
M_01-16-01-000 |
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
3021 |
DWord | Yes |
sercos® III | 8 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 1022 | 4 Byte Signed | Velocity |
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
2858 |
No | 32 bit | Yes |
M_01-16-01-000 |
Related Topics