WS.FORCEOFF
Description
Disables the automatic Wake and Shake procedure if the identified feedback type is sine encoder without halls (FB1.IDENTIFIED = 21) and the encoder pitch is equal to the motor pole pitch of the linear motor.
Value | Description |
---|---|
0 | enabled |
1 | disabled |
General Information
Type |
R/W Parameter |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-16-02-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | No* |
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
EtherCAT COE and CANopen |
541fh/0 |
M_01-16-02-000 |
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
3055 |
Byte | No |
sercos® III | 2 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 1056 | 1 Byte | Integer |
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
---|---|---|---|---|
Modbus |
2926 |
No | 8 bit | No |
Related Topics