AKD Modbus Communication
This manual describes Modbus communication, a simple communication protocol used for reporting data from an industrial device to an HMI or PLC. Download the latest manual from the Kollmorgen website.
AKD EtherCAT Communication

This manual describes the installation, setup, range of functions, and software protocol for the EtherCAT AKD product series. Download the latest manual from the Kollmorgen website.

A PDF format is also available on the disk included with the drive.

AKD CANopen Communication
This manual describes the installation, setup, range of functions, and software protocol for the CANopen AKD product series. Download the latest manual from the Kollmorgen website
A PDF format is also available on the disk included with the drive.
AKD PROFINET
This manual describes the installation, setup, range of functions, and software protocol for the PROFINET AKD product series. Download the latest manual from the Kollmorgen website.
A PDF format is also available on the disk included with the drive.
AKD SynqNet Communication
This manual describes the installation, setup, range of functions, and software protocol for the SynqNet AKD product series. Download the latest manual from the Kollmorgen website.
A PDF format is also available on the disk included with the drive.
AKD EtherNet/IP Communication
This manual describes the installation, setup, range of functions, and software protocol for the EtherNet/IP AKD product series. Download the latest manual from the Kollmorgen website
A PDF format is also available on the disk included with the drive.
EtherNet/IP with Studio 5000
This manual is an easy start guide for using Studio 5000® providing an overview on how to import and configure the AKD and AKD2G Add-On Instructions using Studio 5000, as well as a reference to the Add-On Instructions. Download the latest manual from the Kollmorgen website