AIN#.VALUE

Description

AIN#.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).

Examples

Code

--> AIN1.VALUE
1.420 V

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units V
Range -12.5V to +12.5V
Default Value N/A
Data Type Float
See Also  
Stored in Non Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen AIN1.VALUE 0x3780 0x1 INT 1000:1 - RO True
AIN2.VALUE 0x3781 0x1 INT 1000:1 - RO True