AXIS#.EIP.STREAMING
Description
This parameter retrieves the current streaming state of the drive for the CIP Sync connection. The parameter's value is set to 1 if the drive is currently accepting and acting upon position set-points from the fieldbus master. Otherwise, the value is set to 0.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-11-00-001 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
EtherNet/IP drives: AKD2G-SPI
Fieldbus Information
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.EIP.STREAMING |
7544 |
1D78 |
Unsigned8 |
Read Only |
- |
AXIS2.EIP.STREAMING |
73080 |
11D7 |
Unsigned8 |
Read Only |
- |