AXIS#.FBUS.IL.FF

Description

This parameter displays the current loop feed forward value injected by the fieldbus. The loops are updated every cyclic fieldbus cycle. The fieldbus controller manages jumps in current command due to this feed forward when starting, stopping, switching opmodes, and all other transitions.

Versions

Action Version Notes
Implemented 02-05-05-000

 

General Information

Type

Read/Write

Units

Arms

Range

± Drive peak current (IPEAK)

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.FBUS.IL.FF

5800

16A8

Signed32

Read/Write

-

AXIS2.FBUS.IL.FF

71336

116A

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FBUS.IL.FF

5800

Float

Read/Write

-