AXIS#.FBUS.BLOCKING

Description

The AXIS#.FBUS.BLOCKING command returns the actual protection state if AXIS#.FBUS.PROTECTION is set.

Value Description
0 Commands are not blocked for “service channel” access.
1 Certain commands are blocked and can not be accessed by “service channel” because the fieldbus master has control.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Related Topics

AXIS#.FBUS.PROTECTION

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.FBUS.BLOCKING

5103

13EF

Unsigned8

Read Only

-

AXIS2.FBUS.BLOCKING

70639

113E

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FBUS.BLOCKING

5103

Unsigned8

Read Only

-