AXIS#.IL.FB

Description

This parameter displays the measured actual q-component current reading.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

± Axis peak current (AXIS#.IPEAK )

Default Value

N/A

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen AXIS1.IL.FB 0x500A 0x1 DINT 1000:1 - RO True
AXIS2.IL.FB 0x510A 0x1 DINT 1000:1 - RO True