AXIS#.IL.IVFB

Description

AXIS#.IL.IVFB is an offset value that is added to the measured current in the u-winding of the AXIS#.MOTOR. This value is used for compensating for an error in the current measurement. The drive measures 256 times the current in the u-winding when powering-up the drive. Afterwards, the drive calculates the average value of the measured current and uses this value for the offset value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

A

Range

± Drive peak current (IPEAK)

Default Value

0 A

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Related Topics

Current Loop