AXIS#.IL.LIMITP
Description
This parameter sets the positive user limit clamp value of the torque-producing q-component current command (AXIS#.IL.CMD ). The current command is additionally limited by the motor peak current setting (AXIS#.MOTOR.IPEAK ) and by the present value of the foldback I²t peak motor current protection.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
A |
Range |
0 A to drive peak current (IPEAK) |
Default Value |
Drive peak current (IPEAK) |
Data Type |
Float |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT COE and CANopen | AXIS1.IL.LIMITP | 0x500A | 0x4 | DINT | 1000:1 | - | RW | False |
AXIS2.IL.LIMITP | 0x510A | 0x4 | DINT | 1000:1 | - | RW | False |