AXIS#.JOG.MOVEP

Description

This keyword allows the user to easily start a continuous velocity jog in the positive direction when the user is in Velocity mode or Position mode.

The jog will accelerate/decelerate using AXIS#.JOG.ACC and AXIS#.JOG.DEC. The velocity used is JOG.V. If JOG.V is changed while the jog is in motion, the jog will change its speed to the new JOG.V immediately.

Versions

Action Version Notes
Implemented 02-04-01-000  

General Information

Type Command
Units

N/A

Range N/A
Default Value

N/A

Data Type N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.JOG.MOVEP

6903

1AF7

Unsigned8

Read/Write

-

AXIS2.JOG.MOVEP

72439

11AF

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.JOG.MOVEP

6903

Unsigned8

Read/Write

-