AXIS#.PL.KP
Description
AXIS#.PL.KP sets the proportional gain of the position regulator PID loop.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Hz |
Range |
0 to 500 |
Default Value |
3.27 |
Data Type |
Float |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT COE and CANopen | AXIS1.PL.KP | 0x500C | 0x4 | UDINT | 1000:1 | - | RW | False |
AXIS2.PL.KP | 0x510C | 0x4 | UDINT | 1000:1 | - | RW | False |