AXIS#.PROFINET.SUPPACTUALVALUEDATA
Description
This command can be used to read the cyclic data sent from the drive to the controller in the configured supplemental telegram. Each index reads a 16-bit word in network byte order.
Example
-->AXIS1.PROFINET.SUPPACTUALVALUEDATA
[0] 49191
[1] 0
[2] 112
[3] 57343
[4] 12059
[5] 0
[6] 0
[7] 0
-->AXIS1.PROFINET.SUPPACTUALVALUEDATA 3
57343
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-04-06-000 |
General Information
Type | Read Only |
Units |
N/A |
Range | 0 to 65535 |
Default Value | N/A |
Data Type | Integer |
Stored in Non-Volatile Memory | No |
Variants Supported
PROFINET drives: AKD2G-SPP
Fieldbus Information
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.PROFINET.SUPPACTUALVALUEDATA |
5224 |
Unsigned16[8] |
Read Only |
- |