AXIS#.UNIT.VLINEAR
Description
AXIS#.UNIT.VLINEAR sets the units type for the velocity parameters when the motor type (AXIS#.MOTOR.TYPE ) is linear.
Type |
Description |
---|---|
0 |
counts/s |
1 |
mm/s |
2 |
µm/s |
3 |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 3 |
Default Value |
1 |
Data Type |
Integer |
See Also |
AXIS#.VL.FB , AXIS#.VL.CMDU , AXIS#.VL.CMD, AXIS#.MOTOR.TYPE |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT COE and CANopen | AXIS1.UNIT.VLINEAR | 0x5010 | 0x8 | USINT | - | - | RW | False |
AXIS2.UNIT.VLINEAR | 0x5110 | 0x8 | USINT | - | - | RW | False |