DIO#.SOURCEID

Description

DIO#.SOURCEID sets the digital IO source ID, for sources that require an ID.

Examples

Usage

DIO#.SOURCEID can be used to select the compare channel whenDIO#.SOURCE = 4 (Compare).

Code

The following commands set the source of digital IO 1 to compare channel 1, and digital IO 2 to compare channel 2.

--> DIO1.SOURCE 4
--> DIO1.SOURCEID 1
--> DIO2.SOURCE 4
--> DIO2.SOURCEID 2

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added Compare source 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 0
Data Type Integer
See Also  

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen 0x368A DIO1.SOURCE 0x5 USINT - - RW False
DIO2.SOURCE 0x5 USINT - - RW False
DIO3.SOURCE 0x5 USINT - - RW False
DIO4.SOURCE 0x5 USINT - - RW False
DIO5.SOURCE 0x5 USINT - - RW False
DIO6.SOURCE 0x5 USINT - - RW False