DOUT#.SOURCEID

Description

DOUT#.SOURCEID sets the digital output source ID, for sources that require an ID.

Examples

Usage

DOUT#.SOURCEID can be used to select the compare channel when DOUT#.SOURCE = 4 (Compare).

Code

The following commands set the source of digital output 2 to compare channel 1, and digital output 3 to compare channel 2.

--> DOUT2.SOURCE 4
--> DOUT2.SOURCEID 1
--> DOUT3.SOURCE 4
--> DOUT3.SOURCEID 2

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added Compare channel support 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 0
Data Type Integer
See Also N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen 0x360A DOUT1.SOURCE 0x1 USINT - - RW False
DOUT2.SOURCE 0x1 USINT - - RW False
DOUT3.SOURCE 0x1 USINT - - RW False
DOUT4.SOURCE 0x1 USINT - - RW False
DOUT5.SOURCE 0x1 USINT - - RW False
DOUT6.SOURCE 0x1 USINT - - RW False
DOUT7.SOURCE 0x1 USINT - - RW False
DOUT8.SOURCE 0x1 USINT - - RW False
DOUT9.SOURCE 0x1 USINT - - RW False