EIP.IPMODE
Description
This parameter is used to determine how the drive acquires an IP address for EtherNet/IP communication.
Examples
Usage
0 (default): A static IP address is defined by the value set using EIP.IPADDRESS
1: Acquire a dynamic IP address using BOOTP
2: Acquire a dynamic IP address using DHCP
Code
Set drive to use static IP of 192.168.0.1
--> EIP.IPMODE 0 --> EIP.IPADDRESS 192.168.0.1 --> EIP.IPSUBNET 255.255.255.0 --> EIP.IPRESET
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-06-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 2 |
Default Value |
0 (Static) |
Data Type |
Integer |
See Also |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
EtherNet/IP drives: AKD2G-SPI