EIP.PACKETMISSTHRESHOLD

Description

This parameter defines the threshold of the counter used to trigger F7005 Cyclic Setpoints Missing for EtherNet/IP. The missed packet counter (EIP.MISSEDPACKETCOUNT) increments by 3 on every missed cyclic packet and decrements by 1 when a packet is received. By default, the threshold is set to 9. If the threshold is set to 0, the fault is disabled.

Examples

The following chart provides an example of how the fault counter behaves using the default threshold of 9:

Fieldbus Cycle

Packet Received

Counter

Faulted

0

Yes

0

No

1

Yes

0

No

2

No

3

No

3

Yes

2

No

4

Yes

1

No

5

No

4

No

6

No

7

No

7

Yes

6

No

8

No

9

Yes

9

Yes

8

Yes

10

Yes

7

Yes

11

Yes

6

Yes

Context

EIP.MISSEDPACKETCOUNT

Versions

Action Version Notes
Implemented 02-10-04-000

General Information

Type

Read/Write

Units

N/A

Range

0 (disabled) to 216

Default Value

9

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

EtherNet/IP drives: AKD2G-SPI

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

EIP.PACKETMISSTHRESHOLD

3902

F3E

Unsigned16

Read/Write

-