IP.ADDRESS
Description
This parameter is used to set the IP address of the drive for service port communication when IP.MODE is set to 1 for static IP.
Examples
Usage
IP.ADDRESS is only used when IP.MODE = 1. When setting up the drive with static IP, IP address must be set using IP.ADDRESS and subnet mask must be set using IP.SUBNET. IP.RESET can then be used to apply the specified IP settings.
Code
Set drive to be able to communicate with devices on 192.168.1.x subnet.
--> IP.MODE 1 --> IP.ADDRESS 192.168.0.1
--> IP.SUBNET 255.255.255.0
--> IP.GATEWAY 192.168.1.1
--> IP.RESET
Context
For more information on IP configuration, see Finding and Connecting to a Device.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
|
General Information
Type | Read/Write |
Units | N/A |
Range | 0.0.0.0 to 255.255.255.255 |
Default Value | 0.0.0.0 |
Data Type | String |
See Also | IP.MODE, IP.SUBNET, IP.GATEWAY, IP.RESET |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants supported.