IP.MODE

Description

This parameter is used to determine how the drive acquires an IP address for service port communication.

Examples

Usage

1: A static IP address is defined by the value set using IP.ADDRESS

2 (default): Acquire a dynamic IP address using DHCP or Auto-IP. If a DHCP server is not available, the drive uses Auto-IP to identify and acquire an available IP address.

Code

Set drive to use static IP of 192.168.0.1

--> IP.MODE 1
--> IP.ADDRESS 192.168.0.1
--> IP.SUBNET 255.255.255.0
--> IP.RESET

Context

For more information on IP configuration, see Finding and Connecting to a Device.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 2
Data Type Integer
See Also IP.ADDRESS, IP.SUBNET, IP.GATEWAY, IP.RESET

Stored in Non Volatile Memory

Yes

Variants Supported

All variants supported.

Fieldbus Information

Fieldbus EtherCAT COE and CANopen
Index 525Eh
Subindex 0
Data Type U32
Float Scale N/A
Access Read/Write
PDO Map N/A