MODBUS.WATCHDOG

Description

MODBUS.WATCHDOG is the watchdog timeout in seconds.

The Modbus watchdog fault, F7100, is generated if the drive does not receive any Modbus messages within a time window set by MODBUS.WATCHDOG. Zero disables the watchdog.

Context

For more information, see Handling Broken Connections.

Versions

Action Version Notes

Implemented

02-05-00-000

 

General Information

Type

Read Write Parameter

Units

Seconds

Range

0 to 60

Default Value

5

Data Type

Integer

See Also

Fault F7100

Stored in Non-Volatile Memory

Yes

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

MODBUS.WATCHDOG

3014h

05h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

MODBUS.WATCHDOG

3709

E7D

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

MODBUS.WATCHDOG

3709

Unsigned16

Read/Write

-