PROFINET.USEMODULECFG

Description

This command controls where the drive obtains the telegram configuration. When set to 1 (default), the drive uses the telegram setting from the module configuration in the PROFINET master. When set to 0, the drive uses the telegram setting specified in AXIS#.PROFINET.TELEGRAMID (P922).

Value Description
0

Drive uses the telegram specified from AXIS#.PROFINET.TELEGRAMID (P922)

1

(default)

Drive uses telegram configuration from the sub-module configuration in the PROFINET master.

For more information, see Telegram Mappings.

Versions

Action Version Notes
Implemented 02-04-05-000  

General Information

Type Read/Write
Units

N/A

Range 0 to 1
Default Value 1 (Use sub-module configuration from PLC)
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

PROFINET drives: AKD2G-SPP

Fieldbus Information

PROFINET

Parameter

PNU

Data Type

Access

Units

PROFINET.USEMODULECFG

5211

Unsigned8

Read/Write

-