The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

ACTION#.ACTIVE

Description

Sets whether an action is disabled or enabled. When set to 1, the action will be executed if it is valid.

Value Description
0 Action disabled
1 Action enabled

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen