The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

ACTION#.CONDITIONVALUE

Description

ACTION#.CONDITIONVALUE defines the value used by ACTION#.CONDITION to test against the source. The range of this keyword depends on the value of ACTION#.SOURCE and ACTION#.CONDITION. Both must be set before setting the condition value. If ACTION#.CONDITION is modified, the range of the ACTION#.CONDITIONVALUE may change, and the value will return to default.

Some conditions do not require a condition value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.SOURCE and ACTION#.CONDITION

Default Value

Depends on ACTION#.SOURCE and ACTION#.CONDITION

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen