The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AIN#.OFFSET

Description

AIN#.OFFSET sets the analog offset, which is added to the analog input command to the drive. This value compensates for the analog input signal (AIN#.VALUE) offset or drift.

Examples

Code

--> AIN1.VALUE
0.056 V
--> AIN1.OFFSET -0.056
--> AIN1.VALUE
0.000 V 

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units V
Range -10V to +10V
Default Value 0 V
Data Type Float
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen