The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AOUT#.VALUE

Description

AOUT#.VALUE reads the analog output value.

Examples

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units V
Range 0 to 10V
Default Value 0V
Data Type Float
See Also  
Stored in Non Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen AOUT1.VALUE 0x3800 0x1 INT 1000:1 - RO True
AOUT2.VALUE 0x3801 0x1 INT 1000:1 - RO True

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen