The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.IL.FBSOURCE

Description

This parameter selects the feedback source that current loop uses for commutation angle calculation.

Feedback Sources/Connectors:

1 selects FB1 (connector X1)

2 selects FB2 (connector X2)

3 selects FB3 (connector X23)

4 selects FB4 (connector X21)

5 selects FB5 (connector X22)

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 5

Default Value

1

Data Type

Integer
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
EtherCAT COE and CANopen AXIS1.IL.FBSOURCE 0x500A 0x6 USINT - - RW False
AXIS2.IL.FBSOURCE 0x510A 0x6 USINT - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen