The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.PL.FB

Description

AXIS#.PL.FB returns the position feedback value. The value represents the feedback after the following operations have been performed:

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type

Read Only

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

N/A

Data Type

Float

See Also

 

Stored in Non Volatile Memory

No

Variants Supported

Supported on all variants.

Related Topics

Position Loop


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen