The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.VL.LIMITN

Description

AXIS#.VL.LIMITN sets the velocity command negative limit.

If the input to the velocity loop is lower than AXIS#.VL.LIMITN, then the actual velocity command AXIS#.VL.CMD is limited by the value of AXIS#.VL.LIMITN.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

15000 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

See Also

AXIS#.VL.LIMITP , AXIS#.VL.CMD
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
EtherCAT COE and CANopen AXIS1.VL.LIMITN 0x5011 0x7 DINT - Velocity RW False
AXIS2.VL.LIMITN 0x5111 0x7 DINT - Velocity RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen