The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.WS.CHECKT

Description

This parameter sets the amount of time a commutation error must be present before a fault occurs. Commutation monitoring is disabled when this parameter is set to 0.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

0 to 10,000

Default Value

10

Data Type

Integer
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
EtherCAT COE and CANopen AXIS1.WS.CHECKT 0x5013 0x10 UINT - - RW False
AXIS2.WS.CHECKT 0x5113 0x10 UINT - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen