The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.WS.CHECKV

Description

This parameter sets the velocity threshold which has to be exceeded to activate commutation monitoring.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

N/A

Data Type

Float
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
EtherCAT COE and CANopen AXIS1.WS.CHECKV 0x5013 0xB DINT - Velocity RW False
AXIS2.WS.CHECKV 0x5113 0xB DINT - Velocity RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen