The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.WS.DISTMIN

Description

This parameter sets the minimum movement that is required for commutation finding. If this value is too small, then the commutation finding might fail if too little current is used. The larger this value, the more movement is needed in order to avoid F5500 : "Wake and Shake - Insufficient movement".

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Actual position units

Range

0 to 90 deg

Default Value

1 deg

Data Type

Float

See Also

N/A
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
EtherCAT COE and CANopen AXIS1.WS.DISTMIN 0x5013 0xF DINT - Position RW False
AXIS2.WS.DISTMIN 0x5113 0xF DINT - Position RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen