The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.WS.T

Description

This parameter defines the duration for each different current-vector while the coarse angle calculation. The move distance is proportional to the AXIS#.WS.T and AXIS#.WS.IMAX value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

1 to 200 ms

Default Value

2 ms

Data Type

Integer
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
EtherCAT COE and CANopen AXIS1.WS.T 0x5013 0x4 USINT - - RW False
AXIS2.WS.T 0x5113 0x4 USINT - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen