The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.WS.VTHRESH

Description

This parameter defines the maximum allowed velocity that occurs while commutation finding is active. This supervision runs in real time, but only while wake and shake is active (AXIS#.WS.STATE 2 or greater, for Mode 0). If at any time while wake and shake is running a velocity higher than this value is detected, fault F5503 is generated for over speed. Setting AXIS#.WS.VTHRESH to zero disables this feature. For Mode 1, AXIS#.WS.VTHRESH is only used after the initial phase-finding. 

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

100 RPM

Data Type

Float
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
EtherCAT COE and CANopen AXIS1.WS.VTHRESH 0x5013 0xE DINT - Velocity RW False
AXIS2.WS.VTHRESH 0x5113 0xE DINT - Velocity RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen