The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

AXIS#.CMDSOURCE

Description

AXIS#.CMDSOURCE specifies the source of the command to the axis. AXIS#.OPMODE sets the operation mode to the relevant control loop.

AXIS#.CMDSOURCE values can be set as follows:

Value

Description

0

Service, TCP/IP command

1

Fieldbus command

2

Gearing command

3

Analog command

4

Gantry Mode


  • Only available on Axis 2

If AXIS#.CMDSOURCE is set to 5 then AXIS#.OPMODE must be set to 3.

AXIS#.CMDSOURCE can be changed while the drive is enabled or disabled. If you use the terminal to change the operation mode, it is recommended that you disable the drive before changing the command source.


  • If you change AXIS#.CMDSOURCE from the terminal while the drive is enabled, the system may experience a step change in command.

Example

To set the command source to the TCP/IP channel and the operation mode to velocity:

-->CMDSOURCE 0

-->OPMODE 1

Versions

Action Version Notes
Implemented 02-00-00-000
Value 5 added 02-02-05-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 5

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Related Topics

AXIS#.OPMODE

Gantry Mode


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen