The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

DIO#.SOURCE

Description

Gets or sets the bi-directional output source for channel x when configured as a digital output (see DIO#.DIR).

Value Description
0 - User User controls the output value using DIO#.STATEU
1 - Action Table Action table controls the output value

Examples

Usage

When DIO#.SOURCE = 0 (User) and DIO#.DIR = 1 (output), then DIO#.STATE will be controlled by DIO#.STATEU.

When DIO#.SOURCE = 1 (Action table) and DIO#.DIR = 1 (output), then DIO#.STATE will be controlled by the assigned action, if any.

If DIO#.DIR = 0 (input) then the DIO#.SOURCE parameter is ignored.

Code

Changing output state with STATEU and then changing SOURCE to be action table with no action configured:

--> DIO1.DIR
1 (output)
--> DIO1.SOURCE
0 (user)
--> DIO1.STATE
0
--> DIO1.STATEU 1
--> DIO1.STATE
1
--> DIO1.SOURCE 1 //Action table
--> DIO1.STATE
0

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen DIO1.SOURCE 0x368A 0x5 USINT - - RW False
DIO2.SOURCE 0x368B 0x5 USINT - - RW False
DIO3.SOURCE 0x368C 0x5 USINT - - RW False
DIO4.SOURCE 0x368D 0x5 USINT - - RW False
DIO5.SOURCE 0x368E 0x5 USINT - - RW False
DIO6.SOURCE 0x368F 0x5 USINT - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen