The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

DOUT#.SOURCE

Description

Gets or sets the digital output source.

Value Description
0 - User User controls the output value using DOUT#.STATEU
1 - Action Table Action table controls the output value
2 - Fieldbus Fieldbus controls the output value
3 - Sequencer Sequencer controls the output value

Examples

Usage

When DOUT#.SOURCE = 0 (User), then DOUT#.STATE will be controlled by DOUT#.STATEU.

When DOUT#.SOURCE = 1 (Action table), then DOUT#.STATE will be controlled by the assigned action, if any.

When DOUT#.SOURCE = 2 (Fieldbus), then DOUT#.STATE will be controlled by the fieldbus output control 3601h Digital output control sub 1.

When DOUT#.SOURCE = 3 (Sequencer), then DOUT#.STATE will be controlled by the assigned event in the Sequencer.

Code

Changing output state with STATEU and then changing SOURCE to be action table with no action configured:

--> DOUT1.SOURCE
0 //user
--> DOUT1.STATE
0
--> DOUT1.STATEU 1
--> DOUT1.STATE
1
--> DOUT1.SOURCE 1 //action table
--> DOUT1.STATE
0

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

 

Added fieldbus source 02-00-01-000  
Add Sequencer source 02-02-03-000  

General Information

Type Read/Write
Units N/A
Range 0 to 2
Default Value 0
Data Type Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen DOUT1.SOURCE 0x360A 0x1 USINT - - RW False
DOUT2.SOURCE 0x360B 0x1 USINT - - RW False
DOUT3.SOURCE 0x360C 0x1 USINT - - RW False
DOUT4.SOURCE 0x360D 0x1 USINT - - RW False
DOUT5.SOURCE 0x360E 0x1 USINT - - RW False
DOUT6.SOURCE 0x360F 0x1 USINT - - RW False
DOUT7.SOURCE 0x3610 0x1 USINT - - RW False
DOUT8.SOURCE 0x3611 0x1 USINT - - RW False
DOUT9.SOURCE 0x3612 0x1 USINT - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen