The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

DRV.CUSTOMIDENTIFIER

Description

Use DRV.CUSTOMIDENTIFIER to assign a unique string to a device. The string must use the following formatting rules:

  • ASCII characters only
  • 32 character max length
  • No spaces in string

The string is displayed on the device overview screen and in the start page's device discovery table.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

N/A

Default Value

-

Data Type

String
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
EtherCAT COE and CANopen DRV.CUSTOMIDENTIFIER 0x3000 0x2 STRING(32) - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen