The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

DRV.RUNTIME

Description

DRV.RUNTIME returns the length of time that the drive has been running since it was first activated. This time includes the current session and the total amount of time from all previous sessions.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Days:Hours:Minutes:Seconds

Range

N/A

Default Value

N/A

Data Type

String

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen DRV.RUNTIME 0x3000 0x6 UDINT - - RO False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen