The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

DRV.TEMP

Description

This parameter returns the measured temperature for the specified hardware component.

Examples

Usage

The parameter can be used to track board temperatures as they change during drive operation. There is at least one control board temperature measurement (e.g. DRV.TEMP) and one power board temperature measurement (e.g. AXIS1.TEMP).

Code

--> DRV.TEMP
52.367 (Control) [degC]
--> AXIS1.TEMP
31.664 (Power1) [degC]
--> AXIS2.TEMP
32.312 (Power2) [degC]

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units degC
Range N/A
Default Value N/A
Data Type Float
See Also  

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen